Separate Outputs (SZAHU) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
This option adds two AOs (OAD-O and RAD-O) to provide damper control for the unit mixing dampers. Control dampers in a complimentary fashion and use them as part of the discharge air temperature control strategy along with any heating or cooling coil.