Occupancy Control (SZAHU) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
This section defines how the unit determines occupied status and how it behaves during unoccupied periods. These selections provide the logic for Occupancy Mode Determination. By default a MV network input is added for an Occupancy Schedule (OCC-SCHEDULE).

Override Support adds a network input (OCC-OVERRIDE) which you can use to override the current operating mode.

Occupancy Switch adds a binary input connected to an occupancy sensor that changes the current operating mode.

Setpoint Adjust adds optional setpoint offsets which are to be applied depending on the current occupancy mode.

Temp Occ Support adds a hardware input to support temporary occupancy pushbuttons.

Summer/Winter Compensation Setpoint adds logic which shifts the zone setpoint based on an outdoor air temperature (OA-T) measurement.