Exhaust/Relief Air Damper (SZAHU) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

Supports both analog or two-position dampers. If the system has a building pressure sensor (BLDG-P) then the damper enables whenever its associated supply fan is proven on and modulates to control the building pressure to the set-point (BLDGP-SP), the damper closes when disabled. If there is no building pressure sensor, then the damper position resets based on the minimum outdoor airflow setpoint as determined by ASHRAE 62.1 or California Title 24.