Common Output (SZAHU) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
This option adds a single AO (MAD-O) to provide damper control for mechanically linked dampers or several actuators operating using the same signal. Use the dampers as part of the discharge air temperature control strategy along with any heating or cooling coil.