Single Zone VAV AHU Applications - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Use the Single Zone Air Handling Unit application to program many common Air Handling Unit configurations through the Tool. This application supports the following:
  • Supply fans and return or relief fans
  • Separate or Common OAD and RAD outputs
  • Optional exhaust or relief air damper
  • Support for ASHRAE 62.1 or California Title 24
  • Temperature control strategy
  • Economizer and minimum OA section options
  • Heating and/or cooling coils

See the following sections for information on this application’s logic and selections.