These selections provide the logic to control a Cooling coil.
The selection options for Coils (Cooling) are:
Cooling
- Shutdown on Alarm: This option places the system in shutdown mode when the condensate alarm is active.
-
Cooling Lockout from Outdoor Air
-
Staged Cooling (DX Cooling)
- Device Rotation
- First Stage Modulated
-
Number of Stages
-
One Stage
-
Two Stages
-
Three Stages
-
Four Stages
-
Five Stages
-
Six Stages
-
Seven Stages
-
Eight Stages
-
-
Chilled Water
-
Proportional Actuator
-
Incremental Actuator
-
Two Position Actuator
-
Face and Bypass Damper
-
Proportional Actuator
-
Incremental Actuator
-
-
-
Entering Water Temperature
-
Leaving Water Temperature
-
Coil Pump
-
Pressure/Flow Boost
-
Low Temperature Circulation
-
Pump Status
-
-
Shutdown Strategy
-
Off
-
Protect Coil Based on Outdoor Air Temperature
-
User Defined Position
-
-
Loss of Airflow Strategy
-
Off
-
Remain in Control
-
Protect Coil Based on Outdoor Air Temperature
-
User Defined Position
-
-
Unreliable Sensor Operation
-
Off
-
Hold
-
Protect Coil Based on Outdoor Air Temperature
-
User Defined Position
-
-
The Loss of Airflow Strategy options are available only when the Automatic Restart option for the Supply Fan Status Loss of Airflow Strategy is selected.