These selections provide the option for loading extra, monitor-only sensors.
The selection options for Optional Sensors are:
-
Position Feedback: This option provides feedback inputs for monitoring only purposes. If you want to generate an alarm or other functionality using the position feedback inputs, you must create custom coding to do so.
-
Modulated Damper Outputs
-
No Position Feedback
-
Analog Input per Output
-
Binary Input per Output
-
-
Modulated Valve Outputs
-
No Position Feedback
-
Analog Input per Output
-
Binary Input per Output
-
-
Two Position Damper Outputs
-
No Position Feedback
-
Binary Input per Output
-
Two Binary Inputs per Output
-
-
Two Position Valve Outputs
-
No Position Feedback
-
Binary Input per Output
-
Two Binary Inputs per Output
-
- VSD Outputs
- No Feedback
- Motor Speed (RPM)
- Drive Frequency (Hz)
- Motor Percent (%)
-
-
Outdoor Air
-
Temperature
-
Humidity
-
CO2 Sensor
-
-
Mixed Air
-
Temperature
-
Humidity
-
CO2 Sensor
-
-
Discharge Air
-
Temperature
-
Humidity
-
CO2 Sensor
-
-
Return Air
-
Temperature
-
Humidity
-
CO2 Sensor
-
-
Zone
-
Temperature
-
Humidity
-
CO2 Sensor
-
If a Sensor is required for one of the selections made in the Mechanical System Selection, the option is not available in the Optional Sensors section.