Heating for Zones (MADD-MZ) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

These selections allow the user to specify the type of heat available for each zone as well as to identify the zones that have that heat.

The selection options for Heating for Zones are:

  • Lockout from Outdoor Air

  • Electric Staged

    • One Stage

    • Two Stages

    • Three Stages

  • Hot Water or Steam

    • Proportional Actuator

    • Incremental Actuator

    • Two Position Actuator

  • Zones with Heat

    • Heating Zone One

    • Heating Zone Two

    • Heating Zone Three

    • Heating Zone Four

    • Heating Zone Five

    • Heating Zone Six

    • Heating Zone Seven

    • Heating Zone Eight