These selections provide the option for loading extra, monitor-only sensors.
The selection options for Optional Sensors are:
-
Position Feedback: This option provides feedback inputs for monitoring only purposes. If you want to generate an alarm or other functionality using the position feedback inputs, you must create custom coding to do so.
-
Modulated Damper Outputs
-
No Position Feedback
-
Analog Input per Output
-
Binary Input per Output
-
-
Modulated Valve Outputs
-
No Position Feedback
-
Analog Input per Output
-
Binary Input per Output
-
-
Two Position Damper Outputs
-
No Position Feedback
-
Binary Input per Output
-
Two Binary Inputs per Output
-
-
Two Position Valve Outputs
-
No Position Feedback
-
Binary Input per Output
-
Two Binary Inputs per Output
-
-
-
Outdoor Air
-
Temperature
-
Humidity
-
CO2 Sensor
-
-
Preheat Air Temperature
-
Mixed Air
-
Temperature
-
Humidity
-
CO2 Sensor
-
-
Discharge Air
-
Humidity
-
CO2 Sensor
-
-
Hot Deck
-
Temperature
-
Humidity
-
-
Return Air
-
Temperature
-
Humidity
-
CO2 Sensor
-
-
Misc
-
Heat Recovery Air Temperature
- Mechanical Room Temperature: This option adds an analog input for a zone sensor that monitors the temperature in the mechanical room.
-
If the Zones Only configuration type is selected or if a Sensor is required for one of the selections made in the Mechanical System Selection, the option is not available here.