Summer and Winter Compensation Setpoint Shift (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

Selecting this option shifts the heating and cooling setpoints to compensate for extreme outdoor air temperatures. This works similar to zone control reset by outdoor air temperature, with a large deadband so the setpoints are not modified while the outdoor air is between 50 and 75 °F.