Steam Proportional Valve (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Select this option if your humidifier operates using a steam valve to pump steam directly into the airflow. You may optionally select an Isolation Valve to disable the humidifier when the unit is off.