Wheel Status (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

This option adds a binary input to monitor the status of the heat wheel. If this option is selected, you need to consider a Loss of Status Strategy. This can be either Automatic Restart, which continually attempts to restart the heat wheel until the status indicates it is operating correctly, or Manual Restart, which stops the heat wheel until the alarm is reset. The manual restart option offers a choice of using a network input or Unit Reset Switch (BI) to reset the system.