Economizer Damper(s) (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
These selections provide the logic for the Economizer Dampers. If no economizer control (Free Cooling) is required, these options should not be selected (use Two Position Min OA Damper instead).