Coils (Preheat) (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

These selections provide the logic to control a Preheat coil. A Preheat coil may be located in the Outdoor Air Duct (ahead of the mixing plenum). If this is the case, a Preheat coil is always set to Control to Preheat Air Temperature. When in the Mixed Air Duct, the coil may either be controlled by a dedicated sensor or sequenced with the other devices. During startup, if a DA-T or PH-T sensor is available, the Preheat coil is controlled by the LT-SP (Low Limit Setpoint).