Two Position Actuator (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
Two Position Actuator can be selected if the coil is controlled by a two position valve that uses a binary output to open and close the valve. Two position preheat coil valves are only available with a Face and Bypass Damper to allow some air to bypass the coil in certain conditions. The face and bypass damper can be controlled using a Proportional Actuator or an Incremental Actuator.