Temperature Control Strategy (MADD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
These selections provide the logic for determining the setpoints of the Cold Deck and Hot Deck temperature control loops. The Hot Deck Setpoint options apply only if a Hot Deck heating coil is selected.

The selection options for Temperature Control Strategy are:

  • Fixed Hot, Cold, or both Deck Temperatures

  • Hot, Cold, or both Deck Temperature Reset from OA-T

  • Hot Deck Temperature Reset from RA-T