Select Attribute Dialog Box - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This Select Attribute dialog box is used by the Transfer CAF and Attributes to Controller, Read/Write Attributes Online, and Attribute Template utilities. The dialog box displays a representation of all the possible points in a tree format.

Table 1. Select Attribute Dialog Box

Field

Description

Show All

Use to view all points. If this option is not selected, only BACnet exposed points appear.

Filter Provides a field to search the selection tree based on the node name. The search results include the matching node and its ancestors.

OK

Saves the selections and closes the dialog box.

Cancel

Closes the dialog box without saving.

Opens the Help system.