About this task
The Transfer CAFs to Multiple Controllers option allows you to transfer multiple CAF files to multiple devices on the same trunk and mass edit attributes using attribute templates and read/write functionality. Access this utility from the Tools menu by selecting Trunk Utilities > Transfer CAFs to Multiple Controllers. This menu option is only available when a CAF is not open.
The application files are transferred in series, which can take up to five times longer than the Transfer CAF and Attributes to Controller utility option which transfers application files in parallel.
After selecting the devices and specifying the CAF and attribute template to load, the utility transfers code to the devices in the following order: