Note: If a ZFR1810 Coordinator has Main Code at a version earlier than Release 5.0, it should be upgraded.
- Make sure no CAF is open in the tool.
- From the Tools menu, select Wireless > Upgrade Single ZFR Coordinator.
- In the Connection Parameters, enter the connection parameters:
- For NxE Passthru connections, enter the device hostname or IP address, your user credential, and click Login. Select the correct supervisory device and the trunk.
- For Bluetooth connections, enter the baud rate and COM port information. We recommend you keep the Baud Rate default (38400).
- For MAP 4.2+ / BACnet Router connections, specify the following:
- IP address and UDP port of the router.
- Network number of the MS/TP trunk (1-65,534).
Note: Do not use 1001 for the MS/TP Network Number. The MS/TP Network Number 1001 is reserved for Johnson Controls IP network connections.
- An available Ethernet network interface adapter to use.
Note: If you select an available Ethernet network interface, all IP traffic intended for the MAP 4.2+/ BACnet Router travels through this interface.
When you first open the wizard, the default connection parameters for connecting to a MAP Gateway at version 4.2 are automatically displayed. If the connection parameters are modified, the values are stored in the wizard for future use. To restore the connection parameters to the default values, click the MAP 4.2 Default button.Note: For further information about the MAP and common troubleshooting issues, refer to the Mobile Access Portal Gateway User's Guide (LIT-12011999). - For ZFR dongle connections, enter the PAN Offset.
- In the Discovery section, enter the type of discovery process you want to use: automatic (Auto) and MAC Address. If you selected MAC Address, enter the device address.
- Click Next. The Device Selection Screen appears.
Note: If more than one device has the same Instance Number, the numbers display red in the device list.
- Select the device for ZFR upgrade and click Next. The Summary screen appears.
- Select the Boot, Main, or Radio code to upgrade the ZFR1810 Coordinator.
- Click Finish. The selected device code is transferred to the ZFR Coordinator.
Note: See the Status column of the Operation table and the Status bar for information on the transfer progress and status indicators. When the upgrade completes, the Finish button changes to Done. This change does not happen if you selected the Close wizard after successful transfer check box on the Transfer Summary screen. Instead the wizard closes.
- Click Done.