ZFR Channel Configuration Wizard - Select ZFR Country Code - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This utility has the same Connection and Device Selection screens as the Transfer to Device wizard. See the Transfer Operations section for information on device selection details and connection types and parameters.

Table 1. ZFR Channel Configuration Wizard - Select ZFR Country Code

Item

Description

Country Code

Valid channels where the Wireless Field Bus device is located.

Navigation Buttons

Previous

Moves to the previous screen of the wizard.

Next

Moves to the next screen of the wizard.

Finish/Done

Finish starts the operation.

Done appears in place of Finish after the operation completes and is used to close the wizard.

Cancel

Closes the wizard without performing the operation.

Help

Opens the Help system.