Field | Description |
---|---|
Connection Screen | |
Connection Type | Use to specify the connection type to use:
|
NxE Passthru: Use to specify the following:
|
|
Connection Parameters | Bluetooth: Use to specify the COM port and Baud Rate to use. |
MAP 4.2+ / BACnet Router: Use to specify the following:
When you first open the wizard, the default connection parameters for connecting to a MAP Gateway at version 4.2 are automatically displayed. If the connection parameters are modified, the values are stored in the wizard for future use. To restore the connection parameters to the default values, click the MAP 4.2 Default button.
Note: For further information about the MAP and common troubleshooting issues, refer to the Mobile Access Portal Gateway User's Guide (LIT-12011999).
|
|
ZigBee: Use to specify the Personal Area Network (PAN) offset. | |
Device Selection Screen | |
Discover | Performs a device discovery to find a device. The discovery option only returns ZFR devices that are on the field bus.
Note: After a discovery, when you click Discover again, the list clears from the Device Selection table.
|
Stop | Stops the discovery process. |
Devices Table | Displays the available devices, including:
|
Transfer Summary Screen | |
Device Information | Displays the following device information:
|
Close wizard after successful transfer | Closes the Upgrade Single ZFR Coordinator wizard after successfully completing the transfer operation, when selected. |
Previous | Moves to the previous screen of the wizard. |
Next | Moves to the next screen of the wizard. |
Finish/Done | Finish starts the upgrade process.
Done appears in place of Finish after the upgrade completes and is used to close the wizard. |
Cancel | Closes the wizard without performing the transfer. |
Opens the Help system. |