Sensors (VAV-SD Slave) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The selection options for the Sensors/Inputs are:

  • Supply Air Temperature: This option provides an input for stand-alone morning warm-up logic.

  • Discharge Air Temperature: This option is used primarily as a commissioning check-out feature for applications that have Box Heating to ensure the Discharge Air Temperature increases when Box Heating is commanded on.