VAV Slave Single Duct Applications - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
For single duct slave applications, no zone temperature or setpoint logic is created. Instead, Network Input points read corresponding values using peer-to-peer references from the associated Master VAV application to track key Mode states, inputs for CO2 and OA Percent, Flow Status and % Command, and any heating outputs from the master VAV box. Using this technique to control the VAV slaves ensures that the master and slave boxes are synchronized to heat and cool the entire space.