Supply Air Temperature (VAV-SD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Select this option to add a temperature sensor to the inlet of the VAV box to monitor primary inlet air temperature.

If you choose this option, you can also use this value to determine when morning warm-up mode is applicable by selecting the Used for Morning Warm-up check box. Warm-up logic assumes that the air handling unit supplies hot air during the warm-up cycle to the associated VAV Box. Typically, morning warm-up logic is initiated through a Network Input for morning warm-up, which is a selection in the Optional Features (VAV-SD) section of the tree. If the Supply Air Temperature Used for Morning Warm-up option is selected, the option under Optional Feature for Network Warmup - Cooldown Support is not required.