This option is used primarily as a commissioning check-out feature for applications that have Box Heating to ensure the Discharge Air Temperature increases when Box Heating is commanded on. Discharge Air Temperature is also used when Discharge Air Reset by Zone Control is selected in the Box Reheat Coil Control section.