Discharge Air Reset by Zone Control (VAV-SD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This option allows the zone temperature to reset the discharge air setpoint which controls the reheat valve. This application provides much faster control response and can provide much finer control. Discharge Air Reset can provide better control in cases where the reheat valve is too large for the design coil flow,and the control loop can only control a very small portion of the output.