Context-Sensitive Help - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Context-sensitive help functions in multiple ways within the tool. Select a component of the user interface, such as a module, logic block, or dialog box, and press F1 to display the help topic for that selected component. For example, if you select the State Generation Tower Start Determination module and press F1, the Tower Start Determination help topic appears in your default browser. When viewing a dialog box, you can also click the help icon to display the help in your default browser.

When working within the System Selection Wizard, press F1 or click the Help icon () to display application information in the right pane. The upper-right pane includes application help content. The lower-right pane shows the relationship between the node selected in the left pane and other nodes within the tree. See the following figure.

Figure 1. Return Water Temperature Differential Example