System Information Details Dialog - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The System Information Details dialog (formerly the System tab) appears when you click the System Name link below the menu bar or click the System Information link in the status bar. Use the System Information Details dialog to view system-related information.

Table 1. System Information Details Dialog - Configuration Mode

Field

Description

Object - Name

Indicates the name of the System you have open.

Object - Enabled

Indicates if a device has runtime logic enabled.

An enabled status of True indicates that runtime logic is enabled; False indicates that logic has been disabled.

Setup - Revision

Indicates the last time the file was changed structurally.

Setup - Standard Version

Indicates the software version of the tool with which the application was originally built.

Setup - Language

Indicates the language used in the application.

Setup - Unit Set

Indicates the unit set of the devices.

Opens the Help system.

Table 2. System Information Details Dialog - Simulation Mode

Field

Description

Object - Name

Indicates the name of the System you have open.

Object - Enabled

Indicates if a device has runtime logic enabled.

An enabled status of True indicates that runtime logic is enabled; False indicates that logic has been disabled.

Setup - Revision

Indicates the last time the file was changed structurally.

Setup - Standard Version

Indicates the software version of the tool with which the application was originally built.

Setup - Language

Indicates the language used in the application.

Setup - Unit Set

Indicates the unit set of the devices.

Debug - Break Conditions

Use to add, remove, or view details of break conditions.

Debug - Break

Indicates if the system has stopped because of a break condition.

Debug - Debug Mode

Indicates if Debug mode has been activated (Simulation screen).

Debug - Elapsed Debug Time

Indicates the elapsed time the system has been simulating with Debug mode.

Debug - Last Blocks Executed

Indicates the last blocks executed while the system has been simulating with Debug mode.

Operational Data - Execution Run Count

Provides a counter that tracks how many times the control sequence has fully executed.

Operational Data - Average Idle Time

Indicates the EWMA of the percentage of time that the control sequence is not executing, calculated once each minute.

Operational Data - Average Executing Time

Indicates the EWMA of the control sequences total execution time per hour.

Operational Data - Average Execution Frequency

Indicates the EWMA of the number of control sequence executions per hour.

Operational Data - Average Execution Delay

Indicates the EWMA of the time between a request to run by an asynchronous block (including inputs) to when execution starts.

Operational Data - Average Execution Duration

Indicates the EWMA of the time elapsed during a control sequence execution.

Operational Data - Average Slice Count

Indicates the EWMA of the number of times sliced per control sequence execution.

Operational Data - Average Sliced Duration

Indicates the EWMA of cumulative time elapsed during all slices per control sequence execution.

Opens the Help system.

Table 3. System Information Details Dialog - Commissioning Mode

Field

Description

Object - Name

Indicates the name of the System you have open.

Object - Enabled

Indicates if a device has runtime logic enabled.

An enabled status of True indicates that runtime logic is enabled; False indicates that logic has been disabled.

Setup - Revision

Indicates the last time the file was changed structurally.

Setup - Standard Version

Indicates the software version of the tool with which the application was originally built.

Setup - Language

Indicates the language used in the application.

Setup - Unit Set

Indicates the unit set of the devices.

Operational Data - Execution Run Count

Provides a counter that tracks how many times the control sequence has fully executed.

Operational Data - Average Idle Time

Indicates the EWMA of the percentage of time that the control sequence is not executing, calculated once each minute.

Operational Data - Average Executing Time

Indicates the EWMA of the control sequences total execution time per hour.

Operational Data - Average Execution Frequency

Indicates the EWMA of the number of control sequence executions per hour.

Operational Data - Average Execution Delay

Indicates the EWMA of the time between a request to run by an asynchronous block (including inputs) to when execution starts.

Operational Data - Average Execution Duration

Indicates the EWMA of the time elapsed during a control sequence execution.

Operational Data - Average Slice Count

Indicates the EWMA of the number of times sliced per control sequence execution.

Operational Data - Average Sliced Duration

Indicates the EWMA of cumulative time elapsed during all slices per control sequence execution.

Opens the Help system.