Summary Report Options - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
See Printing Summary Reports.

For information on printing the logic diagram, see Printing the Logic Diagram in the Configuring a System section.

Table 1. Summary Report Options

Field

Description

Project Information

Prints the following project information:
  • Software Version
  • Configuration File (CAF, name)
  • Configuration Date
  • Engineering Units (Imperial or Metric from the New System dialog box)
  • Application Name (System Name entered in the New System dialog box; also available on the System tab)
  • Assigned to Controller (list of the hardware devices defined during hardware definition)
  • System Capacity (%)
  • Naming and Signal Preferences (System Defaults or System Defaults/Modified)
  • System Selection Preferences (System Defaults or System Defaults/Modified)

Job Information

Prints the information entered in the Job Information dialog box.

System Selection Summary

Prints the selections made during System Selection.

Controllers

Prints a summary of the hardware network settings, including:
  • Device
  • Address
  • Type (of device)
  • BACnet ID

Inputs/Outputs

Prints a list of all attributes of the hardware point assignments:
  • Label (Input, Output)
  • Object Name
  • Attribute
  • Value
  • Units

Inputs/Outputs Summary

Prints a brief summary of the hardware point assignments:
  • Label (Input, Network Input, Output, and Network Output)
  • Object Name
  • Attribute (Description and Signal only)
  • Value
  • Units

Network Inputs/Outputs

Prints a list of all attributes of the network points:
  • Label (Network Input, Network Output)
  • Object Name
  • Attribute
  • Value
  • Units

Modules

This option is not currently available.

State Tables

Prints the State Tables.

Unit Validation

Prints a brief summary of the Units:
  • Name (Module) for Activity (includes these classes: Reliability Merge, Last Value, Totalization, Comparison 2, MUX 2) and Passthru (includes Inputs and Outputs)
  • Name (Logic Block)
  • Default Value (Current value in Commissioning mode)
  • Units

Parameters

Prints the Parameters list, including:
  • Item (Module Type, Module Name, and Parameters) for Activity (includes these classes: Reliability Merge, Last Value, Totalization, Comparison 2, MUX 2) and Passthru (includes Inputs and Outputs)
  • Default Value
  • Standard Name

Connections

Prints the Connections tables, including the following for each table:
  • Source Block and Port
  • Selected Module Input and Output
  • Destination Block and Port

Duplicate Names

Prints a list of duplicate objects, including:
  • Object name
  • Object Type
  • Standard Name

OK

Creates a report of the selected data in PDF format that you can print and/or save.

Cancel

Closes the dialog box without creating a printable PDF.

Opens the Help system.