System - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
In the tool, a system is represented by the mechanical equipment and the logic needed to control that equipment, independent of hardware definition. The System Selection Wizard describes the make-up of a mechanical system to aid you in creating the group of logic components that work together to control the mechanical system. See System Types and Configurations in the Configuring a System section.