The Features panel appears across the bottom of the Classic View workspace. You can view this panel regardless of the application tab that currently appears.
Different trees and features appear depending on if the controller is an Advanced Application, General Purpose, or VAV Controller.
Depending on the mode in which the tool is operating, you are able to perform certain tasks in the Features Panel. For information on the modes, see the Modes section. The following table describes the tasks you can perform in the panel in the different modes.
Task |
Mode |
||
---|---|---|---|
Configuration |
Simulation |
Commissioning |
|
View Connections |
X |
X |
X |
Modify Connections |
X |
||
View Parameters |
X |
X |
X |
Modify Parameters 1 |
X |
X 2 |
X2 |
Configure the Display (Display) |
X |
||
View the State Tables |
X |
X |
X |
Modify the State Tables |
X |
||
View Advanced Program Features |
X |
X |
|
Modify Advanced Program Features |
X |
X 3 |
|
View BACnet Exposed Information |
X |
X |
X |