This module category appears on the left side of the Control tab below the Inputs category (Figure 1). These modules are used for override monitoring. A miscellaneous input reads the current Present Value and Priority of PAO, AO, and BO objects.
Note:
Override monitoring is not available during Simulation mode.
See Miscellaneous Input Modules for information.
Back to Control Tab Module Categories