Application - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

An application is a collection of the components that make up the control logic of a system, including modules, logic blocks, custom logic, and hardware definition. For information on the types of applications you can create, see Applications .