User Interface - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This tool is used to configure, simulate, and commission devices, such as field controllers, I/O Modules, and VAV Box Controllers. The tool operates in three modes: Configuration, Simulation, and Commissioning.

This section describes the UI of the tool when you are viewing an application using one of the standard perspectives (user interfaces)—Classic View and Simple View. Components of the UI can vary depending on your view and if you have configured a customized perspective, but the functionality of these components is the same.

For information on perspectives, see Perspectives.

For information on the tasks you can do in these views, see the Configuring a System, Simulating a System, and Commissioning a System sections.

Before performing tasks in the tool, see the Getting Started section for guidance.