Backup Files - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
When you upgrade your system, the tool creates a backup version of the original file and stores the file in the same directory as the original file. The backup file has the same name as the original file; however, the backup file has a .bak extension. To use the backup file, you need to remove the extension from the file name.

Note: The default location of a CAF is C:\Users\username.