Coils (UV) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The separate selections for Cooling and Heating Coils allow for either staged, proportional, or on-off outputs.

The selection options for Coils are:

Cooling

  • Condensate Alarm: This option adds a binary input for a condensate sensor that shuts down the cooling system when activated.
    • Shutdown on Alarm: This option places the system in shutdown mode when the Condensate Alarm is active.
  • Cooling Lockout from Outdoor Air: This option creates Network Inputs for Cooling Lockout Setpoints along with an Outdoor Air Temperature Network Input. If this option is not selected, then Cooling Enabled Network inputs are created. All created Network Inputs interface to the Cooling Availability Determination State Generators, which are always used as State Table Interfaces to the Staged Compressor Control (Heat Pump Staged Compressors v51) Output Controllers.

  • DX Cooling

    • One Stage

    • Two Stages

    • Three Stages

  • Cold Water

    • Proportional Actuator

    • Incremental Actuator

    • Two Position Actuator

Heating

  • Heating Lockout from Outdoor Air: This option creates Network Inputs for Heating Lockout Setpoints along with an Outdoor Air Temperature Network Input. If this option is not selected, then Heating Enabled Network inputs are created. All created Network Inputs interface to the Heating Availability Determination State Generators, which are always used as State Table Interfaces to the Staged Compressor Control (Heat Pump Staged Compressors v51) Output Controllers.

  • Electric Staged

    • One Stage

    • Two Stages

    • Three Stages

  • Hot Water or Steam
    • Proportional Actuator

    • Face and Bypass Damper: This option modulates a Face and Bypass Damper in conjunction with Two Position Control logic for the Heating Coil. The position of the face and Bypass Coil in conjunction with the Cooling Coil configures a setting on the UV Face and Bypass Heating Control Output module to determine the control action of the Face and Bypass Damper.

      • Proportional Actuator

      • Incremental Actuator

    • Incremental Actuator

    • Face and Bypass Damper: This option modulates a Face and Bypass Damper in conjunction with Two Position Control logic for the Heating Coil. The position of the face and Bypass Coil in conjunction with the Cooling Coil configures a setting on the UV Face and Bypass Heating Control Output module to determine the control action of the Face and Bypass Damper.

      • Proportional Actuator

      • Incremental Actuator

    • Two Position Actuator

      • Face and Bypass Damper: This option modulates a Face and Bypass Damper in conjunction with Two Position Control logic for the Heating Coil. The position of the face and Bypass Coil in conjunction with the Cooling Coil configures a setting on the UV Face and Bypass Heating Control Output module to determine the control action of the Face and Bypass Damper.

        • Proportional Actuator

        • Incremental Actuator

      • Configuration

        • Cooling Coil in Same Path as Heating

        • Cooling Coil in Separate Path from Heating

  • Common Heating-Cooling: If you select either one of the Cooling or Heating Coil options, this option is not available.

    • Condensate Alarm: This option adds a binary input for a condensate sensor that shuts down the cooling system when activated.
      • Shutdown on Alarm: This option places the system in shutdown mode when the Condensate Alarm is active.
    • Proportional Actuator

    • Incremental Actuator

    • Two Position Actuator

    • Summer-Winter Changeover Switch: This option provides a Binary Input to determine the control action of the coil.