Economizer Suitability (UV) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Economizer Suitability selections are not available when ASHRAE Cycle 1 is selected. Otherwise, the Economizer Availability Determination Setpoint module is created and interfaced to the choice selected.

The selection options for Economizer Suitability are:

  • Network Command

  • Binary Input (Enthalpy Switch)

  • Outdoor Air

    • Dry Bulb Temp Economizer

    • Temp & Enthalpy Economizer