The following table describes the attributes used by the Staged Device Enable Determination Parallel module.
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
Fan Mode |
Indicates whether the fan is currently commanded on. |
Off Set Name: Off/On |
|
State |
G |
Provides the desired status to Staged Enable. |
False Set Name: False/True/Fault |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)