Module Use in Applications (Autocalibration Sequence) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Autocalibration Sequence Use in Application System Selection Trees

Module Instance Name

Applications

Autocalibration Sequence

All VAV Applications

To see a module's connections and how modules interact with it, view the Connections table.