Module Use in Applications (Fan Determination [VAV Parallel Temp Based]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the name in the following table.

Table 1. Fan Determination (VAV Parallel Temp Based) Uses in Application System Selection Trees

Module Instance Name

Applications

Parallel Fan Determination Temp Based

VAV Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.