Module Use in Applications (Unoccupied Sequencing [VAV]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Unoccupied Sequencing (VAV) Uses in Application System Selection Trees

Module Instance Name

Applications

VAV Unocc Status Determination

VAV Single Duct Applications

VAV Dual Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.