Module Use in Applications (Unoccupied Sequencing [AHU Mixed Air ZN-T]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Unoccupied Sequencing (AHU Mixed Air ZN-T) Uses in Application System Selection Trees

Module Instance Name

Applications

Zone Unoccupied Sequencing

AHU Mixed Air Single Duct Applications

AHU Rooftop Unit Applications

To see a module's connections and how modules interact with it, view the Connections table.