Table 1 describes the attributes used by the State Generation Last Value (Boolean, Enum, Float) modules.
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
Input |
Passes the Default Value to the Present Value on the first execution after startup or enable. Otherwise the Current Value of the Input is passed to the Present Value. |
False 1st Enum 0.0 |
|
Present Value |
G, V |
Output of this module. |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)