Module Use in Applications (Unit Enable Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Unit Enable Determination Uses in Application System Selection Trees

Module Instance Name

Applications

Unit Enable Determination

All Air Handling Unit Applications

Fan Coil Applications

Heat Pump Applications

Unit Ventilator Applications

VAV Single Duct Applications

VAV Dual Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.