The following table describes the attributes used by this module.
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
EFF-OCC (Effective Occupancy) |
G, V |
The resultant Occupancy Mode of the control system as determined based on the input values. |
Set Name: Occ Effective |
OCCMODE-BYPASSTIME (Bypass Time) |
V |
Length of time that the Bypass mode remains active, once activated. |
3600 Seconds |
Occupancy Override |
SC |
Contains the highest priority in controlling the effective occupancy output. It typically is controlled by the user directly commanding the input. |
Not Set Set Name: Occ Override |
Occupancy Schedule |
SC |
Contains the third highest priority in controlling the effective occupancy output. It typically is controlled by a schedule in the supervisory system. |
Not Set Set Name: Occ Schedule |
Occupancy Sensor |
SC |
Indicates when someone is in the space or whether the space should be considered occupied. |
Not Set Set Name: Occ Sensor |
Temporary Occupancy |
SC |
Represents a local momentary button that allows occupants to indicate their presence. |
Inactive Set Name: Inactive/Active |
State |
V |
Indicates which input is presently driving the Effective Occupancy |
Occupancy Override Set Name: Occupancy Effective State |