Module Use in Applications (Occupancy Mode Determination [MZ]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Occupancy Mode Determination (MZ) Uses in Application System Selection Trees

Module Instance Name

Applications

Occupancy Mode Determination (MZ)

AHU Multizone (Mixed Air Dual Duct) Applications

To see a module's connections and how modules interact with it, view the Connections table.