Occupancy Mode Determination (MZ) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This module extends the base Occupancy Mode Determination module with support for a Temporary Occupancy input for up to eight zones (with the zone number designated here by X, representing zones 1-8). You can view and modify this module; however, you cannot change the key behavior performed by the Occupancy Mode Determination module.