Primary States (Fan Alarm Status) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
When the Fan Alarm from the command hierarchy is True the module output is latched in an Alarm state until reset by the reset input.

Table 1. Fan Alarm Status Command Hierarchy

Fan Mode

Flow Status

Fan Alarm

Off

*

False

On

NOT Fault

False

Fault

True