Module Use in Applications (Fan Alarm Status) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Fan Alarm Status Uses in Application System Selection Trees

Module Instance

Applications

Fan Alarm Status

Heat Pump Applications

Unit Ventilator Applications

To see a module's connections and how modules interact with it, view the Connections table.