Reliability (Energy Hold Off Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Table 1. Energy Hold Off Determination Reliability

Input

Behavior When Input Is Not Reliable

Hardware Mode

Specifies that when the Hardware Reliability is False the State output matches the Network Mode if the Network Reliability is True. If both Hardware Reliability and Network Reliability are False, the output is Normal.

Network Mode

Specifies that when the Network Reliability is False the State output matches the Hardware Mode if the Hardware Reliability is True. If both Hardware Reliability and Network Reliability are False, the output is Normal.